{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
TSXETC101 Explicit Messaging CIP Modbus Object Write Example

Issue
The attached document is a CIP Modbus Object Write example for a TSXETC101 using the Send_Req block to write to a Quantum 140NOC77101.


Product Line
This program will read from located registers in Schneider PLC's with the following network modules installed:

  • 140NOC77101
  • BMXNOC0401
  • TSXETC101
Do not use this example to read from located registers in Schneider PLC's through the following network module:
  • 140NOC78000


Resolution
See attachment: TSXETC101_CIP_Modbus_Object_WRITE_Example.pdf


Legacy KB System (APS) Data: RESL210427 V1.0, Originally authored by DaDz on 01/25/2013, Last Edited by DaDz on 01/25/2013
Related ranges: Modicon Premium

Schneider Electric Saudi Arabia

Attachment(s)
TSXETC101_CIP_Modbus_Object_WRITE_Example.pdf [131.71 KB]