Issue
The attached document is a CIP Modbus Object Read example for a TSXETC101 using the Send_Req block to read from a Quantum 140NOC77101.
Product Line
Premium TSXETC101
Quantum 140NOC77101
M340 BMXNOC0401
Resolution
This example will read from located registers in Schneider PLC's with the following network modules installed:
- TSXETC101
- 140NOC77101
- BMXNOC0401
This example does not apply to reading from located registers in Schneider PLC's through the following network module:
- 140NOC78000
(Removed File URL: 210428_45B6/TSXETC101_CIP_Modbus_Object_READ_Example.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/b0d88c9927345b0dc1257afe002cc849/fl_block_5/0.120?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL210428 V1.0, Originally authored by DaDz on 01/25/2013, Last Edited by DaDz on 01/25/2013
Related ranges: Modicon Premium
Released for:Schneider Electric Saudi Arabia
Issue
The attached document is a CIP Modbus Object Read example for a TSXETC101 using the Send_Req block to read from a Quantum 140NOC77101.
Product Line
Premium TSXETC101
Quantum 140NOC77101
M340 BMXNOC0401
Resolution
This example will read from located registers in Schneider PLC's with the following network modules installed:
- TSXETC101
- 140NOC77101
- BMXNOC0401
This example does not apply to reading from located registers in Schneider PLC's through the following network module:
- 140NOC78000
(Removed File URL: 210428_45B6/TSXETC101_CIP_Modbus_Object_READ_Example.pdf)(Removed Image URL: /PubResEXPORT.nsf/2b87ee90be777fc085257c28006ee4ef/b0d88c9927345b0dc1257afe002cc849/fl_block_5/0.120?OpenElement&FieldElemFormat=gif)
Legacy KB System (APS) Data: RESL210428 V1.0, Originally authored by DaDz on 01/25/2013, Last Edited by DaDz on 01/25/2013
Related ranges: Modicon Premium