The scale factor for the Energy reading in the Series 700 Power Meter is automatically adjusted by the meter. The front display will adjust based on the range of the reading. There is a scale register associated to Energy but is not user adjustable. Energy is stored in a 2 register format as a floating point value. Other Meters like the Series 2000, 3000, 4000 Circuit Monitors and the Series 800 Power Meter store Energy in 4 registers with a Modulo 10,000 (mod10) format.
Original article# 4712
Date Created: Unknown
Last Revised: March 19, 2008
Public
Original Author: PMOZONE
All content © 1992-2008 Schneider Electric
Legacy KB System (APS) Data: RESL184650 V2.0, Originally authored by DaMi on 06/17/2007, Last Edited by PhHa on 03/20/2008
Related ranges: PM700 series
Released for:Schneider Electric Saudi Arabia