Issue
There are no webpages in the EGX100 and EGX300 for the CM100/200 Series Meters
Product Line
EGX100
EGX300
Webpage Generator Software
Environment
Webpage of the EGX100 and EGX300
Cause
Expected Behavior
Resolution
The EGX100 and EGX300 does not have webpages built into it for those meter types.
The Web Page Generator Software is a software that makes custom webpages for the gateway, but it does not provide support for the Series 100 and 200 Circuit Monitors.
Released for:Schneider Electric Saudi Arabia