Product Line:
Enercept and Energy Meter
Resolution:
Follow the steps below in the example to convert register values to an integer.
In this example register 287 has a value of 17395 and register 288 has a value of -22528. Register 287 is the upper 16 bit number and 288 is the lower 16 bit number.
1) Convert 17395 and 22528 to binary numbers (add a 0 to the front of the number to make it 16 bits) and combine them (drop the negative sign from register 288). This will give you the following binary number:
0100001111110011 0 101100000000000
2) Drop the 0 to the far left giving you:
1000011111100110101100000000000
3) Take the 8 bits on the far left and convert them to a decimal number:
10000111 | 11100110101100000000000
10000111 = 135
4) Subtract 127 from the value that you got in step 3:
135 - 127 = 8
5) Take the part of the binary number that was not used in step 3
11100110101100000000000
6) Count over from the left the amount calculated in step 4. Drop off everything to the right of this.
11100110
7) Add a 1 to the front of that number.
111100110
8) Convert that number to decimal and this is the register value.
486
Released for: Schneider Electric Saudi Arabia










Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.