{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Vigilohm EM9B: clarification on frequency operating range

Goals and Symptoms

Is it possible to take our vigilohm EM9B with the reference number 50557 for voltage 200VAC / 380-800Hz as the frequency range shows in catalog is 50-60-400-1000Hz.

Facts and Changes

Keywords: EM9B, Vigilohm, Frequency range, range of frequencies, operating range, range of operation, frequency spectrum

Causes and Fixes

In catalog, frequency range of EM9B is shown as 50-60-400-1000Hz. This means it will work on all frequencies from 50 to 1000Hz.


  • Last Revised: 14-Feb-08

    Public

    All content © 1992-2008 Schneider Electric


Legacy KB System (APS) Data: RESL191087 V1.0, Originally authored by KBAdPM on 02/16/2008, Last Edited by KBAdPM on 02/16/2008
Related ranges: Vigilohm

Schneider Electric Saudi Arabia

Explore more
Range:
Vigilohm
Explore more
Range:
Vigilohm
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.