{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to configure a TesysT on Profibus with Siemens Step7

Goals and Symptoms


This document will describe you how to configure TeSysT on a network Profibus with a PLC Siemens S300 station. The CPU is a CPU 315 - 2 DP with Profibus port embedded.

We use Simatic S7, STEP 7 V5.4 SP3. Into Simatic you have two sub-softwares to configure the Profibus Network : NetPro and HW Config.
NetPro: you define which kind of product you need on your Profibus network (TesysU, TesysT…)
HW Config:

    • PLC hardware configuration
      Configuration for each device Network (TesysT with or without expansion module, which control unit for TesysU and which information you want to exchange on the network)

Causes and Fixes

This document will describe you how to configure TeSysT on a network Profibus with a PLC Siemens S300 station. The CPU is a CPU 315 - 2 DP with Profibus port embedded.

We use Simatic S7, STEP 7 V5.4 SP3. Into Simatic you have two sub-softwares to configure the Profibus Network : NetPro and HW Config.
NetPro: you define which kind of product you need on your Profibus network (TesysU, TesysT…)
HW Config:

    • PLC hardware configuration
      Configuration for each device Network (TesysT with or without expansion module, which control unit for TesysU and which information you want to exchange on the network)

Schneider Electric Saudi Arabia

Attachment(s)
Files_R036.7z [853.46 KB]