{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is Blokset compliant with fire resistance/retardant rules?

There is no particular fire test or rules for Blokset as a switchboard, but all the insulating and plastic parts must follow the rules defined in standard IEC 61439-1 item 10.2.3.3.


  • The insulating parts are tested according to IEC60695-2-11 and with the following values:
      • Glowing/hot-wire test 960°C 30/30s for insulating parts in contact with live parts

        Glowing/hot-wire test 650°C 30/30s for insulating parts not in contact with live parts.

        FAQ Is Blokset compliant with fire resistanceretardant rules.pdf


Legacy KB System (APS) Data: RESL199754 V2.0, Originally authored by JoElRe on 08/29/2009, Last Edited by GwPo on 07/23/2010
Related ranges: Blokset

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.