{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the Export Control Classification Number (ECCN) for ION meters or ION/SPM/PME software?

Issue
What is the Export Control Classification Number (ECCN) for ION meters or ION/SPM/PME software?

Product Line
ION, ION Enterprise, Struxureware Power Monitoring, Power Monitoring Expert

Environment
Power Monitoring Software and Hardware

Resolution
The Export Control Classification Number (ECCN) for ION meters or ION/SPM/PME Software is EAR99.

ECCN determines whether a license is needed to export dual-use items (i.e. commodities, technology and software that have both civilian and military or proliferation applications) outside of the U.S. This number appears in the Commerce Control List (CCL) provided by the Bureau of Industry and Security (BIS) within the U.S. Department of Commerce. These controls are implemented through the Export Administration Regulations (EAR).

For more details, please refer to:

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: