{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is there a version of AR7580A, AR7585 or AR7588 with 4" cable guides or can it be field modified?
Issue:
There is need for a shallower version of the finger-style cable managers.

Product Line:
NetShelter High Capacity Cable Managers

Environment:
All versions and serial ranges.

Cause:
The 6 inch cable guides of the AR7580A, AR7585 or AR7588 are too deep.

Resolution:
Schneider Electric does not currently offer a shallower version of these cable managers but they can be field modified to 4" cable guides.
This requires replacing the cable guides of an AR7580A with the 4" cable guides of the AR7721.
For the AR7585 the cable guides are replaced with AR7722.
For the AR7588 the cable guides are replaced with AR7723.

For instructions please see the attached file.

Schneider Electric Saudi Arabia

Attachment(s)
20140124 Field Modification of AR7580A 4in Cable Guides Rev4.pdf [162.44 KB]