Search FAQs
Is there a deeper version of the AR7711?
Issue:
The PDU needs to be mounted deeper than AR7711 allows.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
The installation requires a deeper bracket.
Resolution:
There's not a deeper version of the AR7711, but two brackets can be combined to increase the depth of the furthest 0U mounting hole to approx. 5.7".
See attached file
The PDU needs to be mounted deeper than AR7711 allows.
Product Line:
NetShelter SX
Environment:
All versions and serial ranges.
Cause:
The installation requires a deeper bracket.
Resolution:
There's not a deeper version of the AR7711, but two brackets can be combined to increase the depth of the furthest 0U mounting hole to approx. 5.7".
See attached file
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Explore more
Range:
Explore more
Range: