{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Loading settings onto a VAMP relay that doesn't have the same complete part number.

Issue
May the settings file from a VPG210-001361 be directly loaded into a VAMP 210-5A7ADA-3.20 using VAMPset?

Product Line
VAMP relays

Resolution
If the complete part numbers doesn't match one cannot load the same setting file to each other.  Each VAMP relay will have to be manually configured.
Also if the unit has the same part number and firmware is not the same one cannot load the setting file.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: