{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATS22 operate at 50 deg C temperatures?

Article available in these languages: Spanish

Issue:
Operating temperature range for the Altistart 22

Product Line:
ATS22, Altistart 22

Environment:
All models, all serial numbers.

Cause:
high or low ambient temperatures.

Resolution:
The standard current ratings for the ATS22 is based on an ambient temperature of 40C (104F).

The minimum operating temperature is -10C (14F).  The maximum operating temperature is 60C (140F).
When operating above 40C (104F), the softstart needs to be derated by 2.2% for every degree Celsius above 40C (104F).

For example:  ATS22D32S6U is 32A rated.  For an ambient temperature of 50C (122F), derating is 22% (2.2 x 10).  The 32A softstart rating becomes 24.96A (32A x 0.78 = 24.96).

Schneider Electric Saudi Arabia