{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Why the vfd will not ramp to the correct speed of the 0-10V signal on AI1?

Issue:
The analog input signal do not match what is being sent.

Product line:
Altivar 61/71

Environment:
All models, all serial numbers

Cause:
The AI1 input is a bipolar input.  If AI1 negative is not referenced to common the drive is looking for a range of 20 V dc ( +10 to  - 10).

Resolution:
Verify the factory installed jumper between AI1- and common terminals is installed.

Schneider Electric Saudi Arabia