What is the solution for SIL2 or SIL3 Emergency Stop function ?
Thanks to Check the Attachment for Safety-related stop function initiated by Emergency stop push button which minimize the consequences of possibly harmful event.
Released for:Schneider Electric Saudi Arabia
Attachment(s)
Emergency Stop SIL2 and SIL3.pdf [242.51 KB]
Explore more
Range:
VigiPacT
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.