Issue
After connecting a VAMP 10L (VAM10LSE) module to a VAMP 321 the error light is illuminated.
Product Line
VAMP 321
VAMP ARC Flash Modules
Cause
The VAMP module must be configured to talk to the VAMP 321. Until this communication connection is established the VAMP 10L module will be in an error status. (This is also for any other ARC Flash Module)
Resolution
Connect to the VAMP 321 using the VAMPset software. Navigate to the ARC Protection screen, then click on the Install arc sensors and I/O units > select install, then write the changes to the VAMP 321. The VAMP 321 will locate all I/O devices along with any connected sensors.
Released for: Schneider Electric Saudi Arabia






Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.