{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What type of registers can the SoMachine Modbus serial IO Scanner of a M238 / M258 / LMC058 / M241 / M251 read or write?

The SoMachine Modbus IO Scanner for serial communication can only read or write holding registers, also called 4x registers or %MW registers. If other types of registers have to be read or written, a Modbus Manager along with Read_Var / Write_Var function blocks has to be used. One serial port can be programmed to handle either one Modbus IO Scanner or one Modbus Manager along with Read_Var / Write_Var function blocks. You cannot program one serial port of a M238 / M258 / LMC058 / M241 / M251 to handle both.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Saudi Arabia