{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can I connect a USB Barcode Scanner to a HMISTU655/855?

Issue:
Can I connect a USB Barcode Scanner to a HMISTU655/855?

Product Line:
HMIS5T, HMISTU655, HMISTU855

Resolution:
The HMISTU655/855 USB port does not have enough power to fully power up the USB Barcode scanner.

Your two options would be to use a USB hub that have an external power or use the advanced panel Magelis that have enough power on the USB port.

Schneider Electric Saudi Arabia