{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I use SoMove with the ATV212 drive?

Issue:
ATV212 use with SoMove.

Product Line:
Altivar 212

Environment:
All serial numbers

Cause:
Customer wanted to use SoMove to program ATV212, but the ATV212 was not listed in the SoMove device options.

Resolution:
SoMove should work with the ATV212 drive, if the ATV212 Drives firmware is V5.1 or higher.
Link to Somove and DTMs: https://www.se.com/us/en/product-range/2714-somove/#software-and-firmware

Schneider Electric Saudi Arabia