{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What does a flashing H mean on the ATV21 and ATV212 Drives?

Issue:
Flashing H on the ATV21 and ATV212 Drives

Product Line:

Altivar 21 and 212

Environment:
All

Cause:
Flashing H and he drive resets

Resolution:
The flashing H means the drive controller is approaching an overheating fault.
Check the heat sink cooling on the drive.  If this is a S-Flex, check for anything that might restrict air flow near the top of the drives vent as well as checking the drive's cooling fan.

Schneider Electric Saudi Arabia