{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the Modbus port on a Unity Momentum considered Modbus Port 1 when using an XMIT instruction ?

Issue
What are the Modbus port designations on a Unity Momentum M1 and M1E

Product Line
Unity Momentum, Unity Pro

Resolution
When using a Unity Momentum M1, the Modbus ports are designated as MB port 0 and MB port 1.
When using a Unity Momentum M1E, the Modbus port is designated as MB port 0.

Schneider Electric Saudi Arabia