Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can all 8 channels of a BMXART0814 module be used to read thermocouples without the ABE7CPA412 block for cold junction compensation?

Issue

Can the BMXART0814 module be used without the ABE7CPA412 and maintain use of all 8 channels for Thermocouple operation?

Product Line

Modicon M340, Modicon M580, X80 IO.

Resolution

Yes. Using a 2-wire PT100 RTD wired to channel 4 on terminals EX+ and EX-. This will allow all 8 channels of the BMXART0814 to be used for thermocouple operation as configured and with a single  CJC from Channel 4. Channel 4 will have the 2-wire RTD on EX+ and EX- and the TC on MS+ and MS-.

Schneider Electric Saudi Arabia

How can all 8 channels of a BMXART0814 module be used to read thermocouples without the ABE7CPA412 block for cold junction compensation?

Issue

Can the BMXART0814 module be used without the ABE7CPA412 and maintain use of all 8 channels for Thermocouple operation?

Product Line

Modicon M340, Modicon M580, X80 IO.

Resolution

Yes. Using a 2-wire PT100 RTD wired to channel 4 on terminals EX+ and EX-. This will allow all 8 channels of the BMXART0814 to be used for thermocouple operation as configured and with a single  CJC from Channel 4. Channel 4 will have the 2-wire RTD on EX+ and EX- and the TC on MS+ and MS-.

Schneider Electric Saudi Arabia

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.