{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATV71 have a function for up and down speed using logic inputs?

Issue:
Controlling motor speed through logic inputs on the ATV71.

Product Line:
Altivar 61, Altivar 71

Environment:
All models and serial numbers.

Cause:
None

Resolution:
The function [+/- Speed] will allow motor speed to be increased or decreased using logic inputs.  The following parameters apply:

NO. MENU SUB-MENU CODEADJUSTDESCRIPTION
1.6COMMAND------------------RFCCh2 activeRef. 2 switching
1.6COMMAND------------------FR2+/- speedReference 2 Channel
1.7APPL FUN+/- SpeedUSPLix+ speed assign.
1.7APPL FUN+/- SpeeddSPLIx- speed assign.
1.7APPL FUNReference SavedStrEEpromFreq. reference stored

Schneider Electric Saudi Arabia