Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
        
How can we help you today?
What processor are used in the Preventa XPSMF35 Safety controller?
Issue
What processor are used in the Preventa XPSMF35 Safety controller

Product Line

XPSMF35 

Resolution

The XPSMF35 controllers are equipped with 2 microprocessors for the safety-related processing (CPU) and 1 microprocessor for the communications (COM).

The CPU and COM Processors are 32-bit processors.

 

CPU: Motorola Coldfire MCF 5206e

Clock Speed: 40 MHz / 36 MIPS (54 Mhz / 50 MIPS)

 

COM: Motorola Power PC 860

Clock Speed: 50 MHz / 66 MIPS (66 Mhz / 88 MIPS) 

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: