{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the address of the Com Scanner input and Com Scanner output on the ATV61 / ATV71 Series Drives?

Article available in these languages: Spanish

ISSUE:
Needs the register address for the data from the Com Scanner input and Com Scanner output on the ATV61 / ATV71 Series Drives

Product Line:
Altivar 61 / Altivar 71 series drives.

Environment:
All models, All serial numbers.

Cause:
Drive is configured for communication control via the com scanner input and output but the base address of the com scanner input and output is unknown.

Resolution:
The base address of the com scanner input is 12741.
The base address of the com scanner output is 12761.

Schneider Electric Saudi Arabia