Search FAQs
What is the operating temperature of the ATV71?
Issue:
Altivar 71 operating temperature.
Product Line:
ATV71 Altivar 71
Environment:
All
Cause:
Verify application requirements.
Resolution:
Ambient air temperature around the device :
Operation °C
For ATV 71H..... and ATV71P....N4Z drives: - 10…+ 50 without derating, depending on the rating. Up to + 60°C with derating (and with control card fan kit VW3 A9 4.. depending on the rating).
For ATV 71W.... drives: - 10…+ 40 without derating.
Storage °C - 25…+ 70
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: