{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the ATV312 have a run time or elapsed time meter?

Issue:
Run time on ATV312

Product Line:
Altivar 312

Environment:
All models

Cause:
None

Resolution:
Yes, parameter rtH (Operating time) in the SUP menu displays the total time that the motor has been powered up.  If desired, this can be set as the default display.  This operating time can be reset to zero by setting rPr = rtH in the FLt menu.

Schneider Electric Saudi Arabia

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: