{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the types of available Vigi Modules to be installed with NSX MCCB for Earth leakage protection?

The types of available Vigi Modules to be installed with NSX MCCB for Earth leakage protection are:

- Vigi ME which is a fixed Module (cannot adjust sensitivity)

- Vigi MH - Adjustable from 0.03 to 10 A and used with NSX 100-160-250 Frames

- Vigi MB adjustable from 0.3 to 30 A and used with NSX 400-630 Frames

Schneider Electric Saudi Arabia