Issue:
PID control setup on ATV21 and ATV212 drives?
Product Line:
Altivar ATV21 and ATV212, S-Flex enclosed.
Environment:
All
Cause:
Setting up PID control on the ATV21 and ATV212 drives.
Resolution:
- Press the mode button until you see AUF
- Arrow down to F------ and press enter
- Find F360 and press enter choose your PID feedback assignment and to activate your PID function
- 1 for VIA
- 2 for VIB
- Set to 3 if you want to use the up and down arrows as your set point.
- Set to 1 for VIA or 2 for VIB if you want your analog input to be your set point.
Please note: it is not a good idea to set up to set your PID feedback F360 to 1 VIA and your set point FNOD to 1 VIA.
Basic setup for a 4-20mA signal input for PID feedback would be:
F201=20% (4mA)
F202=0
F203=100% (20mA)
F204= 60hz
F360= 1 (enable PID and feedback is VIA 4 to 20mA)
FNOD= 3 (up and down arrows are your set point.
Optional settings:
F362=PID proportional gain
F363= PID integral gain
F380 = 1 for Reverse acting (0 = deactivated)
Ref manual 30072-451-63
Released for: Schneider Electric Saudi Arabia


Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Search FAQs
Search topic-related frequently asked questions to find answers you need.
Contact Sales
Start your sales enquiry online and an expert will connect with you.