Search FAQs
Can an ATV212 24Vdc power supply from P24 be used for logic inputs on another ATV212 drive?
Issue:
P24 vdc signal from one ATV212 drive to start another ATV212 drive
Product Line:
Altivar ATV212
Environment:
All
Cause:
Needs to use only one power signal to start two drives.
Resolution:
Yes. Jumper together a CC terminal from both drives so that they both have the same ground reference.
Note: The P24 power supply is limited to 200mA. Each logic input consumes about 5mA.
P24 vdc signal from one ATV212 drive to start another ATV212 drive
Product Line:
Altivar ATV212
Environment:
All
Cause:
Needs to use only one power signal to start two drives.
Resolution:
Yes. Jumper together a CC terminal from both drives so that they both have the same ground reference.
Note: The P24 power supply is limited to 200mA. Each logic input consumes about 5mA.
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: