Issue:
ATV32 Devicenet Programming
Product Line:
Altivar 32
Environment:
All ATV32 drives with Devicenet option card VW3A3609.
Cause:
Programming assistance
Resolution:
CONF enter
FULL enter
CON enter
CbD enter
Communications settings
AdrC= address= set 0-63
bdr= Bit rate= Auto, 125K 250K,500K choose one
bdrU= Data rate= Auto, 125K, 250K, 500K choose one
C1DA= Assembly set up= 20, 21, 100, unconfig choose one
OCA1 and OMA1 are for assemblies 100 and 101 only.
See page 20 of 88 in the manual. https://www.se.com/us/en/download/document/S1A28702/
Released for:Schneider Electric Saudi Arabia