{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What alarms can be automatically reset on a High Capacity Uniflair Unit

Issue:
This article contains what alarms can be automatically reset on a High Capacity Uniflair Unit.

Product line:
High capacity Models 4500/5000.

Environment:
All Serial Numbers.

Cause:
Install.

Resolution:

The Automatic Reset allows the unit to clear the alarm and continue operation if the alarm condition is no longer present.

• High/Low Temperature Threshold Exceeded

• High/Low Humidity Threshold Exceeded

• Supply Air Temperature Threshold Exceeded

• High/Low Airflow

• Humidifier

• Smoke Detected

• Electric Heater Over Temperature

• Electronic Expansion Valve Error

• Low Pressure

• Circuit 1 Chilled Water High Temperature Threshold Exceeded

• Circuit 1 Chilled Water Temperature too High for Dehumidification

• Insufficient Chilled Water Flow

• Primary/Secondary Power Source Unavailable

• Dual Circuit Expansion Board Error Detected

• Digital 2/4/6 Input Abnormal

• External Sensor Threshold Exceeded

Schneider Electric Saudi Arabia