{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
TSXSCP114 and TSXSCP1114 serial communications baud rate ranges
Issue
This Resolution clarifies the baud rate ranges for the TSXSCP114 and TSXSCP1114 RS422/RS485 Serial Communication cards.


Product Line
TSXSCP114
TSXSCP1114


Resolution
Unity allows the user to select the same baud rate ranges between the TSXSCP114 and TSXSCP1114 even though their baud rate ranges are different.  Unity does not limit the selection of the baud rates based on the communication card configured.

The baud rate ranges are as follows:

TSXSCP114 - 1200, 2400, 4800, 9600, 19200

TSXSCP1114 - 1200, 2400, 4800, 9600, 19200, 38400, 57600

The default baud rate is 9600.

Reference Premium and Atrium using Unity Pro Asynchronous Serial Link User Manual, 12/2018.  Part number, 35006178.16.

Schneider Electric Saudi Arabia