Issue
What is the maximum number of variables in Web Designer application for a TSXWMY100 module.
Product Line
TSXWMY100
Environment
Windows 7, Windows 8
Resolution
The maximum number of WORD type variables that can be defined in a Web Designer application for a TSXWMY100 module is 1000. If STRING type variables are used, the device 'Variables' table namespace in a Web Designer application for a TSXWMY100 module is limited to a total of 2000 bytes. If the 'Variables' table contains a mixture of WORD and STRING type variables, the limit is still 2000 bytes. Any attempt to exceed the limit could result in communications issues with the Web Designer services.
This limit is due to the available memory in the module and cannot be changed.
Released for:Schneider Electric Saudi Arabia