{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you install both the Ethernet IP and the Ethernet TCP/IP option cards on the ATV61/71 at the same time?

Issue:
Wondering if you can install both the Ethernet IP and the Ethernet TCP/IP option cards on the ATV61/71 at the same time?

Product Line:
Altivar ATV61 ATV71 with Ethernet TCP IP VW3A3310D or IP VW3A3316 option cards.

Environment:
All

Cause:
Can you have both Ethernet option cards installed at the same time?

Resolution:
No,  You can not install the VW3A3310D and the VW3A3316 cards at the same time.  You must install one or the other.

Schneider Electric Saudi Arabia