Issue:
Motor Rated Current adjustment range on the ATS22.
Product Line:
Altistart 22 ATS22
Environment:
All models
Cause:
What range of motors can be used for a particular ATS22 model
Resolution:
The Motor Rated Current, In, is adjustable from .4x to 1.0x the ATS22 current rating, IcL.
In other words, it can be adjusted down to 40% of the ATS22's rating.
Eg: An ATS22C17S6U, rated 170A, has an In range of 68 - 170A.
Released for:Schneider Electric Saudi Arabia