{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Altivar drives state when the auto decel ramp adapt feature bRA is engaged?
Issue:
Drives state when the auto decel ramp adapt feature is engaged
Product Line:
Alitvar ATV61, ATV71, ATV312, ATV31, ATV58, ATV12
Environment:
All
Cause:
Needs to know the status of the drive when auto decel ramp adapt is activated.
Resolution:
When the stop order is given, the drive state is "DEC" and if this is needed (brA=Yes) the drive will raise the deceleration time but the state stays to "DEC" until the motor is stopped then the state goes in "rdY".

Schneider Electric Saudi Arabia

Attachment(s)
brA settings.pdf [79.98 KB]