Search FAQs
Micom S1 studio error during front port connection "port is busy" OR "cannot open port"
Title:
Micom S1 studio error during test connection "port is busy"
Issue:
When trying to connect to a Micom relay using the front panel with the correct communication parameters, the below errors are noticed during a "new connection" or "Test Connection"
![Connection parameters Connection parameters](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zqAYQAY&oid=00DA0000000abSm)
![Test Connection Test Connection](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zpQWQAY&oid=00DA0000000abSm)
Product Line:
Micom S1 Studio
Micom relays
Environment:
Micom front port communication
Cause 1:
The software was able to successfully connect up the first time and has locked the communication port from further use.
Cause 2:
The same communication port is being used by some other process.
Resolution 1:
This can occur when a 'cross-over' cable is used to communicate with the relay i.e. one that connects Tx to Tx and Rx to Rx. To determine the actual pinout required for the cable please follow What is the RS232 communication pinout for the Micom Relays?
Resolution 2:
Open Device Manager to make sure the USB to RS232 converter being used is connected to the proper com port being used in the software.
a. Device manager can be accessed by right clicking on "My Computer" from the desktop icon or "Computer" from the start menu.
b. Make sure the com port being used by the USB to RS232 converter is the same as that being used to connect using Micom S1 studio as shown below
![Device Manager Device Manager](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000008zq6JQAQ&oid=00DA0000000abSm)
Micom S1 studio error during test connection "port is busy"
Issue:
When trying to connect to a Micom relay using the front panel with the correct communication parameters, the below errors are noticed during a "new connection" or "Test Connection"
Product Line:
Micom S1 Studio
Micom relays
Environment:
Micom front port communication
Cause 1:
The software was able to successfully connect up the first time and has locked the communication port from further use.
Cause 2:
The same communication port is being used by some other process.
Resolution 1:
This can occur when a 'cross-over' cable is used to communicate with the relay i.e. one that connects Tx to Tx and Rx to Rx. To determine the actual pinout required for the cable please follow What is the RS232 communication pinout for the Micom Relays?
Resolution 2:
Open Device Manager to make sure the USB to RS232 converter being used is connected to the proper com port being used in the software.
a. Device manager can be accessed by right clicking on "My Computer" from the desktop icon or "Computer" from the start menu.
b. Make sure the com port being used by the USB to RS232 converter is the same as that being used to connect using Micom S1 studio as shown below
Released for:Schneider Electric Saudi Arabia
Explore more
Range:
Explore more
Range: