{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Stabiloy cables with Altistart Soft starts

Issue:
Can you use Stabiloy?

Product Line:
Altistart Soft starts

Environment:
All

Cause:
Stabiloy is an Aluminum/Copper Hybrid

Resolution:
Per the Installation Manual, Only Copper Cables are compatible with Schneider Electric Soft start terminals.  Can use Stabiloy only on the high hp range that require lugs.  You will, however, have to use Stabiloy compatible lugs to use those cables.
Aug 2014, Per US Engineering.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: