Issue:
Overvoltage level on an ATV61/ATV71 that causes OSF
Product Line:
Altivar 61 and Altivar 71 series drives.
Environment:
All part numbers ending with M3XXX or N4XXX, All serial numbers.
Cause:
N/A
Resolution:
- The over supply flag OSF FAULT is set when the drive is in the capacitor charging state and the dc bus voltage is higher than OSFH_Level.
Overvoltage level on an ATV61/ATV71 that causes OSF
Product Line:
Altivar 61 and Altivar 71 series drives.
Environment:
All part numbers ending with M3XXX or N4XXX, All serial numbers.
Cause:
N/A
Resolution:
- The over supply flag OSF FAULT is set when the drive is in the capacitor charging state and the dc bus voltage is higher than OSFH_Level.
- The over supply flag OSF FAULT is set when the drive is in the PWM deactivated state and when the dc bus voltage is higher than OBFH_Level.
- The flag OSF FAULT is reset when the dc bus voltage is lower than OSFL Level.
- The over supply detection is always activated and cannot be inhibited.
Released for:Schneider Electric Saudi Arabia