{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: What causes USF Undervoltage on an ATS22 Soft Starter?

Article available in these languages: French, Dutch

Issue:
Why is USF displayed on Altistart 22?

Product Line:
Altistart 22 ATS22

Environment:
All models, All serial numbers.

Cause:
USF is being triggered when the starter is supplied with proper power.

Resolution:
USF is an Undervoltage Fault.  Basically, the incoming supply voltage is too low.

The following parameters affect the USF fault:
-In the ConF menu,
UIn should be set to the nominal incoming 3 phase voltage.
The factory default is 480V for S6 and S6U ranges, and 400V for Q range.
-In the PrO menu,
USd ( Under Voltage Threshold ) sets the threshold as a percentage of parameter UIn.
USt  (Under Voltage Time Delay ) sets the amount of time delay in seconds until a USF trip.  The voltage must remain under the threshold for the entire delay to activate the fault.

Note that the under voltage protection feature becomes operational only after a run command has been issued.When voltage drops to zero, the soft starter will trip immediately, overriding the time delay.
An isolation contactor that is not pulling in with run command applied can also cause USF as the main power to the soft start is not made.

Example:
Uln= 480V, USd = 70%, USt = 5 seconds.   So, if after a run command is issued, the incoming voltage drops to less than 336 volts (480V * 70%)  and stays there for more than 5 seconds, USF will be triggered.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: