{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the Com'X 200/210 or Com'X 510 support the Powerlogic and SY/MAX protocols?

Issue
A user needs to know if the Com'X 200 / Com'X 210 / Com'X 510 supports the Powerlogic and SY/MAX protocols

Product Line
Com'X 200/EBX200
Com'X 210/EBX210
Com'X 510/EBX510

Environment
Gateway Portocol Support

Cause
A user needs to convert legacy device protocols such as Powerlogic and SY/MAX from CM2000 series, CM200 series, CM100 series, etc. to Modbus TCP/IP.

Resolution
The Com'X 200, Com'X 210 and Com'X 510 do not support the Powerlogic or SY/MAX protocols.
Use an EGX100 or EGX300 to convert Powerlogic or SY/MAX to Modbus TCP/IP. However, EGX100/300 have been obsoleted and the replacement is EGX150. EGX150 supports the Powerlogic or SY/MAX protocols as well.

Com'X 200 supported Protocols:
IPv4
IPv6 - HTTP
HTTPS
Modbus TCP/IP

Com'X 510 supported Protocols:
HTTP
HTTPS
FTP
SMTP
Modubs TCP/IP

Schneider Electric Saudi Arabia