Issue:
Configuration the ATV61 and ATV71 drive to start stop with the HMI and use AI2 for 4-20mA speed control.
Product Line:
Altivar ATV61 ATV71
Environment:
All
Cause:
Wants to start and stop the drive with his remote keypad display and use his 4-20mA signal for speed control.
Resolution:
Program the drive as follows
Drives MENU
Simply Start Menu 1.6
Ref 1 channel is AI2
Profile is set to SEP ( Separate)
CMD switching set to Channel 1 active
CMD channel 1 set to HMI
Released for:Schneider Electric Saudi Arabia