{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do we have a module in the M340 or M580 family which will read type B,R or S thermocouples ?

We have two modules which will read these types of thermocouples. The 4 channel BMXART0414 and the 8 channel BMXART0814.
These modules will not only support the Platinum/Rhodium type B, R and S but types E, J,  K, L, N, U and T. These modules will
also provide RTD capability for Pt (Platinum) , Cu (Copper) and Ni (Nickel).




R-82917

Schneider Electric Saudi Arabia