Issue:
Torque control not working
Product Line:
ATV71
Environment:
All models and serial numbers
Cause:
Motor control type not set to SVCI
torque/speed not enabled [Trq/spd switching]
Torque reference channel not assigned [Torque ref. channel]
Speed reference not assigned
Resolution:
Set motor control type t SVCI
Enable torque speed switching. Set to "Yes" for permanent torque control or assign a logic input.
Assign a torque reference channel. This can be set as the low speed, preset speed, analog input, serial comm or encoder feedback.
Assign a speed reference (do not assign it to the same as torque reference channel)
Torque control not working
Product Line:
ATV71
Environment:
All models and serial numbers
Cause:
Motor control type not set to SVCI
torque/speed not enabled [Trq/spd switching]
Torque reference channel not assigned [Torque ref. channel]
Speed reference not assigned
Resolution:
Set motor control type t SVCI
Enable torque speed switching. Set to "Yes" for permanent torque control or assign a logic input.
Assign a torque reference channel. This can be set as the low speed, preset speed, analog input, serial comm or encoder feedback.
Assign a speed reference (do not assign it to the same as torque reference channel)
Released for: Schneider Electric Saudi Arabia


Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.