{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are my options to have Modbus RTU on a TSX Premium controller?
Issue:
What are my options to have Modbus RTU on a TSX Premium controller?

Product Line:
TSXP57, Premium,

Environment:


Cause:


Resolution:
There are two options for Modbus RTU for the Premium PLC.  There is a RS232 and a RS485 PCMCIA cards.
For RS232 modbus PCMCIA card, the part number is TSXSCP111. There are two cables available for the PCMCIA card, TSXSCPCD1030 (3m) or TSXSCPCD1100 (10m).  The cable has a DB25 on the end.

For RS485 modbus PCMCIA card, the part number is TSXSCP114 .  There are two cables available for the PCMCIA card,TSXSCPCM4030 (3m RS485 2-wire with flying leads on the end) or TSXSCPCM4530 (3m RS485 2-wire or 4-wire with DB15 on the end).

Schneider Electric Saudi Arabia