{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to register an ION service
Issue
An ION Service is removed after installation or does not get installed

Environment
Command Prompt running as administrator

Product
ION Enterprise 6.0
StruxureWare Power Monitoring (SPM) 7.0
Power Monitoring Expert 7.2
Power Monitoring Expert 8.x
Power Monitoring Expert 9.x
Power Monitoring Expert 2020
Power Monitoring Expert 2021​​​​​​​
Power Monitoring Expert 2022
Power Monitoring Expert 2023

Cause
Many different reasons could cause an ION service to not exist. If the issue is during the installation process it is recommended to contact technical support for assistance.

Resolution
Any of the ION services can be registered from the command line by running:
"-Service"
and unregistered with:
"-UnregServer"

The EXE files are located in \system\bin folder.
Below is an example of registering the OPC service.

Command Prompt Example to Register a Service

Below is a list of the executables associated with each ION service. Not all services are available in each version of the software:
ServiceExecutable
ION Alert MonitorAlertMonitor.exe
ION Cloud AgentCloud.Agent.Pme.Service.exe
ION Component IdentifierPMLexeMonikers.exe
ION Connection ManagementPMLConnectionManager.exe
ION Diagnostics and UsageIONDiagnosticsAndUsage.exe
ION Event WatcherIONEventWatcherService.exe
ION Log Inserterlogsrv.exe
ION Log Subsystem RouterLogSubsystem.Service.exe
ION Managed CircuitLogicalDevice.AutoConfig.ServiceHost.exe
ION Network RouterPMLNetman.exe
ION OPC Data AccessION.OpcDaServer.exe
ION Power Quality AggregationIONPowerQualityAggregator.exe
ION PQDIF ExporterPQDIFExporter.exe
ION QueryQueryServer.exe
ION Real Time DataIONServices.exe
ION Report SubscriptionIONReportSubscriptionService.exe
ION Sitesiteserv.exe
ION Software Alarm or
ION Software Data Processing
DataProcessorService.exe
ION Software Modbus GatewayModbusGatewayService.exe
ION Virtual Processor vip.exe
ION XML Subscription WebReach.XMLSubscriptionService.exe
ION XML Subscription StoreSubscriptionStore.exe


Schneider Electric Saudi Arabia