{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the finger-style vertical cable managers for 600 mm cabinets be installed on the same 0U Accessory Channel as a PDU?

Issue:
Customers may want to mount a PDU on the accessory channel behind the vertical cable manager.

Product Line:
NetShelter SX

Environment:
AR7721, AR7722, AR7723

Cause:
The installation manual of the Cable Managers for 600 mm cabinets shows the cable manager being installed over both PDU mounting areas of the 0U accessory channel.

Resolution:
The vertical cable manager can be installed in the rear-most facing position so that a PDU can be mounted behind it.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: