{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is it possible to change application type of my Sepam?
Issue
Is it possible to change application type of my Sepam

Product Line
Sepam series 20
Sepam series 40
Sepam series 80

Environment
Application Type

Cause
Would like to change the application type of Sepam relay

Resolution
The answer is a little bit different according to the Sepam series:
  • ​Sepam series 20 and 40: Modification of Sepam application type requires replacement of your complete Sepam. You need to order a new Sepam with the correct application type needed.
  • Sepam series 60 and 80: As application type is in the cartridge, modification of Sepam application type requires only replacement of the cartridge. You need to order a new cartridge with the application type needed. Note: be careful, since you may need to purchase additional CCA63x CT adapters, depending on which Application Types are involved.
Note that in all cases, a firmware patch cannot modify application type of a Sepam.

Schneider Electric Saudi Arabia