{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are there any drive configuration settings required when installing a load reactor?

Issue:
What are the programming requirements when installing a load reactor, a motor choke, or output filter?


Product Line:
All Drives


Environment:
All

Cause:
Installation


Resolution:
No, there are no drive settings that have to be changed when using a load reactor.

It would be best to verify with manufacturer of the reactor if they have any limitations on the Switching Frequency or Carrier Frequency, but no changes are required for the drive.

Schneider Electric Saudi Arabia